i.MX6 IPU DIsplay interface sync pulses

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 IPU DIsplay interface sync pulses

965 次查看
andreas81
Contributor I

Hi,

we are working at the moment with i.MX6DL. I tried to setup new display support (RGB interface) in Bootloader U-Boot. There is a struct available, where I can define all the display timings:

.mode= {
.name           = "wvga-rgb",
.refresh        = 57,
.xres           = 800,
.yres           = 480,
.pixclock       = 33260,
.left_margin    = 42,
.right_margin   = 86,
.upper_margin   = 10,
.lower_margin   = 33,
.hsync_len      = 128,
.vsync_len      = 2,
.sync           = 0,
.vmode          = FB_VMODE_NONINTERLACED

But there I miss the activity of the sysnc pulses, e.g. if hsync is active high or active low. I also searched in the user manual about the i.MX6 IPU register where I can set the active high or low information but I can't find it.

So can anybody tell me in which registers I can set the following informations:

V-Sync: Active high or low

H-Sync: Active high or low

Pixel Clock: Data is driven on falling or rising edge

Output enable: Active high or low

Data lines: inverted or not

If anybody can tell me how I can do this in U-Boot it would also help.

Best regards,

Andreas

标签 (2)
标记 (3)
0 项奖励
1 回复

453 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

The HSYNC, VSYNC, Pixel clock polarity was set the register IPU_DI_GENERAL; the DE and data line polarity was set in register IPU_DI_POL.

In followed link, there is sample code to enable the LCD interface display in Uboot: https://community.freescale.com/docs/DOC-98109

0 项奖励