i.MX6 HDMI edgerate setting.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 HDMI edgerate setting.

Jump to solution
655 Views
satoshishimoda
Senior Contributor I

Hi community,

Our patner have a question about i.MX6SDL HDMI.
Please see tx_edgerate[1:0] and ck_edgerate[1:0] in HDMI_PHY_CPCE_CTRL register (chapter 35.7.7 in IMX6SDLRM Rev.1).
They want to know how "override" is used.
I understand if override bit (xx_edgerate[1]) is set, the slow or fast edges setting (xx_edgerate[0]) is enabled, isn't it?
But I don't understand how the edges becomes when the override bit is cleared.
Would you let me know it?


Best Regards,
Satoshi Shimoda

Tags (1)
0 Kudos
1 Solution
556 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Satoshi San,

Yes your understanding it is correct.  If the override bit it is set no matter if you have slow or fast edges settings this are not taking care.

View solution in original post

0 Kudos
2 Replies
557 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Satoshi San,

Yes your understanding it is correct.  If the override bit it is set no matter if you have slow or fast edges settings this are not taking care.

0 Kudos
556 Views
satoshishimoda
Senior Contributor I

Hello jamesbone,

Thank you for your reply.

I understood your reply means "if the override bit is set, slow or fast edges setting is ignored".

But I think "if the override bit is 'cleared', slow or fast edges setting is ignored", right?

Best Regards,

Satoshi Shimoda

0 Kudos