Hi community,
We have some questions about i.MX6SDL HDMI registers of color depth.
Please see the questions as below.
[Q1]
Please see chapter 34.5.39 in IMX6SDLRM Rev.1.
In color_depth[3:0] description, there are two "24 bit per pixel video (8bit per component), 8-bit packing mode", 0000b and 0100b.
Would you let me know whether these two setting are same or not.
If there are not same, please tell me what is different.
[Q2]
Please see chapter 34.5.268 in IMX6SDLRM.
In csc_colorde_pth[3:0] description, there are two "24 bit per pixel video (8bit per component)" same as Q1.
How about this case?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Both options "24 bit per pixel video (8bit per component), 8-bit packing mode",
0000b and 0100b are the same. There are no differences specified.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Both options "24 bit per pixel video (8bit per component), 8-bit packing mode",
0000b and 0100b are the same. There are no differences specified.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------