i.MX6 HDMI color depth registers.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 HDMI color depth registers.

Jump to solution
723 Views
satoshishimoda
Senior Contributor I

Hi community,

We have some questions about i.MX6SDL HDMI registers of color depth.

Please see the questions as below.

[Q1]

Please see chapter 34.5.39 in IMX6SDLRM Rev.1.

In color_depth[3:0] description, there are two "24 bit per pixel video (8bit per component), 8-bit packing mode", 0000b and 0100b.

Would you let me know whether these two setting are same or not.

If there are not same, please tell me what is different.

[Q2]

Please see chapter 34.5.268 in IMX6SDLRM.

In csc_colorde_pth[3:0] description, there are two "24 bit per pixel video (8bit per component)" same as Q1.

How about this case?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (1)
0 Kudos
Reply
1 Solution
619 Views
Yuri
NXP Employee
NXP Employee

  Both options "24 bit per pixel video (8bit per component), 8-bit packing mode",
0000b and 0100b are the same. There are no differences specified.


Have a great day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
620 Views
Yuri
NXP Employee
NXP Employee

  Both options "24 bit per pixel video (8bit per component), 8-bit packing mode",
0000b and 0100b are the same. There are no differences specified.


Have a great day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply