Hi community,
I have a question about i.MX6SDL HDMI.
I have understood i.MX6DL HDMI support 16, 24 bits L-PCM in https://community.freescale.com/thread/349086.
Then, please see chapter 13.2.5 in IMX6SDLLXRM Rev.Rev L3.0.35_4.1.0 (for L3.0.35_4.1.0_BSP).
24 bits audio is not mentioned in this chapter.
In addition, in sound/soc/imx/imx-hdmi-dma.c in L3.0.35_4.1.0, there is the following comment.
/* 24bit not support now. */
So we understood i.MX6SDL supports 24 bits L-PCM, but driver is not supported.
Is this correct?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。