i.MX6 HAB/CAAM self-tests and CAVP validation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 HAB/CAAM self-tests and CAVP validation

1,149件の閲覧回数
awright
Contributor II

I am trying to get FIPS 140-2 certification. Doing so requires the crypto systems to perform known answer tests (KAT) on initialization.  It is my understanding that the bootROM performs a self-test of the CAAM RNG and SHA before performing the HAB authentication. I could not find any details about the self-tests that are being performed. Does it only test the RNG and SHA algorithms?  Does it use standard KAT vectors in the test?

Also, I am looking for a way to perform the CAVP validation tests on the CAAM algorithms. Has Freescale or NXP had the algorithms tested by NIST, as it appears they have done with the PowerQUICC, QorIQ, and StarCore devices?

ラベル(2)
タグ(5)
0 件の賞賛
返信
1 返信

727件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Details of bootROM self-testing are not provided. Nevertheless, You may look

at the “Security Reference Manual for i.MX 6Dual, 6Quad, 6Solo, and 6DualLite”

  In particular - section 5.7.3.2.2 (RNG NIST certification).

https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLSRM&appType=moderatedWithoutFAE&fpsp=1&WT_TYPE...

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信