i.MX6 Ethernet Compliance Testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Ethernet Compliance Testing

1,330件の閲覧回数
kevinharvey
Contributor I

Hello all,

I'm attempting to do some ethernet compliance testing on a Phytec Phyflex i.MX6D SoM.  The compliance software provided by Keysight/Agilent requires the device being tested to transmit scrambled, 3-level random bit sequences to capture the waveforms it needs.  Is there an application available that will accomplish this?  I know some platforms have ethernet utilities that allow the device to enter certain test modes but I'm not having much luck finding anything like that in this case.

Thanks for any help you can provide!

Kevin

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

647件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please note that test pattern for i.MX6 Ethernet Compliance Test is applicable to Phy.

Since i.MX6 has not Ethernet Phy, so this is not applicable to i.MX6.

Please apply to Phy vendor which is used on custom board for Ethernet Compliance

Test data.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信