i.MX6 CPU version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,150件の閲覧回数
vsiles
Senior Contributor I

Hi !

I order to correctly apply some errata, I'd like to check the version/revision of the cortex a9 running on my sabre lite board (boundary devices). From Linux source code and the reference manual, I see that some information seems to be located in the USB_ANALOG:USB_ANALOG_DIGPROG register, but it seems strange to me that such information is located in a USB module.

I'd like to get as much information as possible (revision of the board, the cpu cores, ...) at runtime as possible. Could anyone point me to the correct location for these information ?

Best regards,

Vincent

ラベル(1)
タグ(2)
1 解決策
986件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

USB_ANALOG_DIGPROG can be used  to get information aboutSOC revision. 
NUM_CORES fuse field may be used for further device distinction. Please pay attention,

the DIGPROG has different addresses ; say, for i.MX6 D/Q/S - 0x020C_8260,
but for i.MX6 SL  - 0x020C_8280.

  Also, please use the following :

http://www.nxp.com/files/microcontrollers/doc/eng_bulletin/EB804.pdf 

http://www.nxp.com/files/microcontrollers/doc/eng_bulletin/EB803.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
987件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

USB_ANALOG_DIGPROG can be used  to get information aboutSOC revision. 
NUM_CORES fuse field may be used for further device distinction. Please pay attention,

the DIGPROG has different addresses ; say, for i.MX6 D/Q/S - 0x020C_8260,
but for i.MX6 SL  - 0x020C_8280.

  Also, please use the following :

http://www.nxp.com/files/microcontrollers/doc/eng_bulletin/EB804.pdf 

http://www.nxp.com/files/microcontrollers/doc/eng_bulletin/EB803.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

986件の閲覧回数
vsiles
Senior Contributor I

Thanks you very much.

0 件の賞賛
返信