i.MX6 ARM cores rarely dead locked when communicated with ttymxc0.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 ARM cores rarely dead locked when communicated with ttymxc0.

757 Views
torus1000
Contributor V

Hi,

Two ARM cores dead locked during test command input from console continuously.
It happened once per 24 hours. If dead lock happened, watchdog issue the reset.


Have anyone heard of this phenomenon?


What are the possible causes?

Our board info are as following.

kernel: L3.14.38
Board: Prototype board
host OS: Ubuntu14.04 Lemix(linaro14.04)
Serial port: port1(ttymxc0) 115200bps

Anyone can help me?

Thanks

Labels (3)
Tags (1)
0 Kudos
Reply
3 Replies

625 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Torus,

Did you check this Errata of the device

https://community.nxp.com/message/397208?commentID=397208#comment-397208 

All the ARM errata has been defined in the arch/arm/Kconfig, you can search from the file arch/arm/Kconfig.

 

If you want to see which ERRATA enabled on the i.MX6X, please check the .config file after running the build command: ‘make imx6_defconfig ARCH=ARM ….’

Jaime

0 Kudos
Reply

625 Views
torus1000
Contributor V

Hi Jaime,

I opened new case #00109023 and uploaded register value and system.map.
If you mind, would you reply above case?

Torus

0 Kudos
Reply

625 Views
torus1000
Contributor V

Hi Jaime,

I'm sorry the links you provide give me an error

Unauthorized
This place or content does not exist or access to it is restricted.

Is there any reachable links?

Torus

0 Kudos
Reply