i.MX6 ARM DS-5 debugger doesn't work with kernels after 3.10.53.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 ARM DS-5 debugger doesn't work with kernels after 3.10.53.

584件の閲覧回数
norishinozaki
Contributor V

Hello,

ARM DS-5 debugger works fine with kernel 3.10.17 on i.MX6DL/QSabreSDP

However the version 3.10.53, 3.14.28, 3.14.52 and 4.1.15 doesn't work.

When I connect DS-5 to the running kernel, Sabre hangs.

When I try to boot the kernel with DS-5 connected, it hangs just as explained below.

Is there anyone who knows how to debug(J-TAG) IMX6DL based on 3.14.28 Kernel?

Do I need to change kernel configuration or device tree file?

Should I ask ARM?

BR,

N.S.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

419件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Have you tried to disable CAAM drivers in kernel?

-> Cryptographic API                                

                               [ ] Hardware crypto devices

Luis

0 件の賞賛
返信

419件の閲覧回数
norishinozaki
Contributor V

Hello Luis,

Thanks, I tried with removing the option right now in 3.14.28.
It worked!!

Thank you & BR,

N.S

0 件の賞賛
返信