Hi All !
may you had stuck in a similar problem before and give me a hint on this.
We running a 2.6.35.14 kernel with freescale patches and system become randomly not responding
serial console, fb all frozen.
Magic KeyReq ALT+CTRL+SysReq+<...> give me some idea what happened (see attachment):
We have 2 Gstreamer pipes running a) Audio (audio-pipe) b) Video (video-pipe) both pipes run in its own thread and are fully
independent. If a video is running on the video-pipe, we mute it by set volume to 0 and use the audio-pipe to play an announcement.
Randomly its happen that the system hangs. We get out some infos from the Kernel using the SysReq (see below)
may you can bring light into darkness.
Complete prints attached.
cheers
Chris
Pid: 2325, comm: alsa-sink
CPU: 0 Not tainted (2.6.35.14-ge79684d-dirty #721)
PC is at 0x2ab02018
LR is at 0x2ab02d00
pc : [<2ab02018>] lr : [<2ab02d00>] psr: 20000010
sp : 2f759c88 ip : 00000000 fp : 0006ec84
r10: 00000000 r9 : 00000000 r8 : 00000001
r7 : 00000000 r6 : 000b5e70 r5 : 00000001 r4 : 0006ddc8
r3 : 2ab02018 r2 : 00000000 r1 : 00000000 r0 : 000b5e70
Flags: nzCv IRQs on FIQs on Mode USER_32 ISA ARM Segment user
Control: 10c5387d Table: cfb84019 DAC: 00000015
SysRq : Show clockevent devices & pending hrtimers (no others)
Timer List Version: v0.6
HRTIMER_MAX_CLOCK_BASES: 2
now at 69744121976361 nsecs
and
alsa-sink R running 0 2325 1 0x00000000
[<8002e578>] (unwind_backtrace+0x0/0xf0) from [<8002d88c>] (show_stack+0x10/0x14)
[<8002d88c>] (show_stack+0x10/0x14) from [<8004cb9c>] (show_state_filter+0x58/0xb0)
[<8004cb9c>] (show_state_filter+0x58/0xb0) from [<80247470>] (__handle_sysrq+0xdc/0x1a4)
[<80247470>] (__handle_sysrq+0xdc/0x1a4) from [<80247620>] (sysrq_filter+0xb4/0xc8)
[<80247620>] (sysrq_filter+0xb4/0xc8) from [<802d0254>] (input_pass_event+0x9c/0xec)
[<802d0254>] (input_pass_event+0x9c/0xec) from [<802d23ec>] (input_event+0x74/0xa4)
[<802d23ec>] (input_event+0x74/0xa4) from [<8032d26c>] (hidinput_hid_event+0x2dc/0x330)
[<8032d26c>] (hidinput_hid_event+0x2dc/0x330) from [<80329354>] (hid_process_event+0xfc/0x148)
[<80329354>] (hid_process_event+0xfc/0x148) from [<80329908>] (hid_report_raw_event+0x568/0x58c)
[<80329908>] (hid_report_raw_event+0x568/0x58c) from [<80329abc>] (hid_input_report+0x190/0x1cc)
[<80329abc>] (hid_input_report+0x190/0x1cc) from [<8032eef8>] (hid_irq_in+0x94/0x24c)
[<8032eef8>] (hid_irq_in+0x94/0x24c) from [<802b09d8>] (usb_hcd_giveback_urb+0x70/0xb8)
[<802b09d8>] (usb_hcd_giveback_urb+0x70/0xb8) from [<802bf570>] (ehci_urb_done+0xac/0xc8)
[<802bf570>] (ehci_urb_done+0xac/0xc8) from [<802bf974>] (qh_completions+0x3e8/0x474)
[<802bf974>] (qh_completions+0x3e8/0x474) from [<802c0d7c>] (ehci_work+0x2e8/0x9d4)
[<802c0d7c>] (ehci_work+0x2e8/0x9d4) from [<802c3aac>] (ehci_irq+0x1e4/0x22c)
[<802c3aac>] (ehci_irq+0x1e4/0x22c) from [<802b03b0>] (usb_hcd_irq+0x38/0x90)
[<802b03b0>] (usb_hcd_irq+0x38/0x90) from [<80087708>] (handle_IRQ_event+0x24/0xe4)
[<80087708>] (handle_IRQ_event+0x24/0xe4) from [<80089808>] (handle_level_irq+0xd4/0x180)
[<80089808>] (handle_level_irq+0xd4/0x180) from [<8002906c>] (asm_do_IRQ+0x6c/0x8c)
[<8002906c>] (asm_do_IRQ+0x6c/0x8c) from [<80029a8c>] (__irq_svc+0x4c/0xcc)
Exception stack(0xdfd13b70 to 0xdfd13bb8)
3b60: dfd13bd4 00000000 dfd13e50 00000004
3b80: 00000000 00000001 00000000 dfd13e50 00000001 00000000 00000000 0006e368
3ba0: 159720e0 dfd13bb8 800d12a4 800d0f20 20000013 ffffffff
[<80029a8c>] (__irq_svc+0x4c/0xcc) from [<800d0f20>] (poll_freewait+0x0/0x6c)
[<800d0f20>] (poll_freewait+0x0/0x6c) from [<00000001>] (0x1)
Original Attachment has been moved to: alsa_sink-crash.log.zip
已解决! 转到解答。
Our latest BSP is 11.09 for i.MX53QSB (L2.6.35_11_09_ER_SOURCE). Are you get the latest patches from this release? Also, there is an additional patches for i.MX53QSB (IMX53_LINUX_1109_BSP_PATCH).
You can download them from here:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab
Our latest BSP is 11.09 for i.MX53QSB (L2.6.35_11_09_ER_SOURCE). Are you get the latest patches from this release? Also, there is an additional patches for i.MX53QSB (IMX53_LINUX_1109_BSP_PATCH).
You can download them from here:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab