i.MX53 (or i.MX6) UART and DTE vs DCE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 (or i.MX6) UART and DTE vs DCE

Jump to solution
1,432 Views
mmichaelis
Contributor I

Can anyone explain what use or benefit there is from changing the UART on an i.MX53 from the normal DCE mode to DTE mode?   The documentation is confusing.  Section 76.1.3 says that CTS is an input in DTE mode, but an output in DCE mode.  However, section 76.2.1.2.1 for CTS  says the signal is an output in both DCE and DTE modes.

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
967 Views
igorpadykov
NXP Employee
NXP Employee

yes, you are right

sect.64.2 External Signals IMX6DQRM p.5173

shows that RTS becomes CTS and vice versa.

~igor

View solution in original post

0 Kudos
Reply
5 Replies
967 Views
igorpadykov
NXP Employee
NXP Employee

Hi mmichaelis

there are no special benefits, just direction of some signals are changed

please look at Table 90 "UART I/O Configuration vs. Mode" IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
967 Views
mmichaelis
Contributor I

Does that mean that in DTE mode, the internal CTS logic is connected to the external RTS pin?

0 Kudos
Reply
967 Views
igorpadykov
NXP Employee
NXP Employee

yes, internally CTS logic is connected to the external RTS pin

as shown on sect.64.2 External Signals IMX6DQRM p.5173

Best regards

igor

0 Kudos
Reply
967 Views
mmichaelis
Contributor I

That does not make sense to me.  The UART chapter explains the CTS only in the sense of an output control signal.    There is no explanation of what the CTS does if it is an input.  The same logic applies to the TX and RX lines.    Either something is not explained properly in the documentation, or the UART does not work at all if it is switched to DTE mode.

0 Kudos
Reply
968 Views
igorpadykov
NXP Employee
NXP Employee

yes, you are right

sect.64.2 External Signals IMX6DQRM p.5173

shows that RTS becomes CTS and vice versa.

~igor

0 Kudos
Reply