Can anyone explain what use or benefit there is from changing the UART on an i.MX53 from the normal DCE mode to DTE mode? The documentation is confusing. Section 76.1.3 says that CTS is an input in DTE mode, but an output in DCE mode. However, section 76.2.1.2.1 for CTS says the signal is an output in both DCE and DTE modes.
解決済! 解決策の投稿を見る。
yes, you are right
sect.64.2 External Signals IMX6DQRM p.5173
shows that RTS becomes CTS and vice versa.
~igor
Hi mmichaelis
there are no special benefits, just direction of some signals are changed
please look at Table 90 "UART I/O Configuration vs. Mode" IMX6DQCEC
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Does that mean that in DTE mode, the internal CTS logic is connected to the external RTS pin?
yes, internally CTS logic is connected to the external RTS pin
as shown on sect.64.2 External Signals IMX6DQRM p.5173
Best regards
igor
That does not make sense to me. The UART chapter explains the CTS only in the sense of an output control signal. There is no explanation of what the CTS does if it is an input. The same logic applies to the TX and RX lines. Either something is not explained properly in the documentation, or the UART does not work at all if it is switched to DTE mode.
yes, you are right
sect.64.2 External Signals IMX6DQRM p.5173
shows that RTS becomes CTS and vice versa.
~igor