i.MX53 SMD BSP Chinese Font

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 SMD BSP Chinese Font

Jump to solution
1,066 Views
larson
Contributor III

Hi all,

I use the i.mMX53 SMD BSP and I want the NK support the chinese Font display, I try the all items of the bsp, but only Microsoft YaHei can be displayed, all of others(SimSun & NSimSun/SimSun-ExtB) can displayed by 口口, and in the Microsoft YaHei Font, the FootNotes displayed 口口 too, did i lost something about    the Font items or others items?

By the way, i use the ClearType of the system, but it can not be work, Why?

[HKEY_LOCAL_MACHINE\System\GDI\Gamma]

"Gamma Value"=dword:5dc

[HKEY_LOCAL_MACHINE\System\GDI]

"FontLinkMethods"=dword:00000000

[HKEY_LOCAL_MACHINE\System\GDI\ClearTypeSettings]

"OffOnRotation"= dword:00000000

[HKEY_LOCAL_MACHINE\System\GDI\ClearType]

"ClearType"=dword:00000001

[HKEY_LOCAL_MACHINE\Software\Microsoft\Shell]

"NoClearType"=dword:00000000

Thanks for you help!

Labels (1)
Tags (2)
0 Kudos
1 Solution
785 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

To support Chinese font, you need select the followed items from catalog:

Core OS -> CEBASE -> International -> Local Services

                         National Language Support (NLS)

Core OS -> CEBASE -> International -> Local Specific Support -> Chinese (Simplified)

                         Monotype Imaging AC3 Font Compression

Core OS -> CEBASE -> International -> Local Specific Support -> Chinese (Simplified) -> Fonts -> SimSun & NSimSun

                         SimSun & NSimSun (Subset 2_90)

Then open VS2008 menu "Project" -> IMX53-SMD-Mobility Properties...

In "Configiguration Properties" -> "Locale"; select as attached picture "Locate.png":

View solution in original post

0 Kudos
2 Replies
786 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

To support Chinese font, you need select the followed items from catalog:

Core OS -> CEBASE -> International -> Local Services

                         National Language Support (NLS)

Core OS -> CEBASE -> International -> Local Specific Support -> Chinese (Simplified)

                         Monotype Imaging AC3 Font Compression

Core OS -> CEBASE -> International -> Local Specific Support -> Chinese (Simplified) -> Fonts -> SimSun & NSimSun

                         SimSun & NSimSun (Subset 2_90)

Then open VS2008 menu "Project" -> IMX53-SMD-Mobility Properties...

In "Configiguration Properties" -> "Locale"; select as attached picture "Locate.png":

0 Kudos
785 Views
larson
Contributor III

Hello ,

   Thanks for your help.

    I try it, and find when i don't select the "Multilingual User Interface(MUI)", the display is ok(The Project-> properties is not set) . I do not konw the reason.

0 Kudos