i.MX53-QSB Linux. USB is not working.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX53-QSB Linux. USB is not working.

1,411 次查看
priyathamodela
Contributor I

Hello,

I am using i.MX53 QSB with Linux. I am facing problem with on board USB.

It is unable to populate the device USB devices. I have connected a

Dell Optical mouse(Model: MS111), on the serial console i could see the following prints.

and for about 20 iterations board gets restarted. I am using prebuilt linux images downloaded from freescale.com

usb 2-1: new low speed USB device using fsl-ehci and address 2

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input4

generic-usb 0003:0461:4E22.0001: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 2

usb 2-1: new low speed USB device using fsl-ehci and address 3

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input5

generic-usb 0003:0461:4E22.0002: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 3

usb 2-1: new low speed USB device using fsl-ehci and address 4

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input6

generic-usb 0003:0461:4E22.0003: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 4

usb 2-1: new low speed USB device using fsl-ehci and address 5

input: PixArt USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1:1.0/input/input7

generic-usb 0003:0461:4E22.0004: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-fsl-ehci.1-1/input0

usb 2-1: USB disconnect, address 5


after connecting the device "lsusb" output is

(no device detected)


Bus 001 Device 001: ID 1d6b:0002

Bus 002 Device 001: ID 1d6b:0002

Thanks and Regards

Priyatham.

标签 (3)
标记 (2)
0 项奖励
1 回复

496 次查看
jimmychan
NXP TechSupport
NXP TechSupport

please download the BSP (L2.6.35_11_09_ER_SOURCE) and apply the patches (IMX53_LINUX_1109_BSP_PATCH).

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab

please try to build the image and then run it on the board.

0 项奖励