i.MX50: xx in CKO1_SEL bits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX50: xx in CKO1_SEL bits

Jump to solution
816 Views
norishinozaki
Contributor V

Hello Champs,

I'm going to set CKO1_SEL bits in CCM_CCOSR register by looking at page 360  in i.MX50 RM

What does xx mean ?

pastedImage_0.png

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
1 Solution
710 Views
Yuri
NXP Employee
NXP Employee

xx means that, the value of corresponding bits do not matter - may be any 0 or 1


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
711 Views
Yuri
NXP Employee
NXP Employee

xx means that, the value of corresponding bits do not matter - may be any 0 or 1


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
709 Views
norishinozaki
Contributor V

Hello Yuri,

Thanks always!

Best regards,

Nori Shinozaki

0 Kudos
Reply