Hello Champs,
I'm looking for an address map of fuse bits of BOOT_CFGx in OCOTP.
However I can't find the addresses of BOOT_CFGx.
Seems like OCOTP_CFGx registers are related to.
For example, BOOT_CFG1[7:4] equal to OCOTP_CFG1[7:4]?
Best regards,
Nori Shinozaki
解決済! 解決策の投稿を見る。
Hi Nori
allocation of fuse bits:
OCOTP_CFG3[15:8] | = BOOT_CFG1[7:0] |
OCOTP_CFG3[23:16] = BOOT_CFG2[7:0]
OCOTP_CFG3[31:24] = BOOT_CFG3[7:0]
you can enter ticket (service request) to obtain more full fuse map.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Nori
allocation of fuse bits:
OCOTP_CFG3[15:8] | = BOOT_CFG1[7:0] |
OCOTP_CFG3[23:16] = BOOT_CFG2[7:0]
OCOTP_CFG3[31:24] = BOOT_CFG3[7:0]
you can enter ticket (service request) to obtain more full fuse map.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thanks, So the pads used in muxed 16-bit Nand Flash are;
D[0:15] in the Table 6-9 or A[0:15] as the Table 6-23 describes?
Best regards,
Nori Shinozaki
Hi Nori
I would suggest to create new thread for
this new question and better understand/formulate
question since "muxed 16-bit Nand Flash " is not right
description.
Thanks
igor
Igor,
Thanks!
Ok, this thread was closed.
Best regards,
Nori Shinozaki