Hello Champs,
My cusotmer is designing USB Host(No OTG used) and terminated USB related pins with according to the "Chapter 1 Design Chack List" of the Software Development Guide as follows.
USB_H1_VBUS: 5V supply for USB
USB_H1_RREFEXT: 6.04K Pull-down
USB_H1_GPANAIO: OPEN
USB_OTG_DP, DN, ID, VBUS, RREFEXT, GPANAIO: OPEN
Is it Ok to follow SDG for designing USB Host?
Because I heard i.MX50 EVK and the SDG were designed before the datasheet is fixed.
Best Regards,
Nori Shinozaki
Hi Nori
it is Ok to follow SDG for designing USB Host,
also example of USB Host can be found in
i.MX50 EVK Board Schematics : i.MX50 Quick EVK board Design Files
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
They refer the schematics.
However the EVK USB is designed to be used in OTG mode.
These 6 pins are not figured out how to terminate in Host mode.
USB_OTG_DP
DN
ID
VBUS
RREFEXT
GPANAIO
Are they OK with OPEN in Host Mode as in the OTG?
Best regards,
Nori Shinozaki