i.MX35 PDK -> DZ60 MCU Source Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX35 PDK -> DZ60 MCU Source Code

ソリューションへジャンプ
1,158件の閲覧回数
g_moreno
Contributor III

Hello. Where can I find the S08DZ60 source code for the i.MX35 PDK? This MCU is used in the CPU board to provide software and hardware support for several peripherals. Any help would be greatly appreciated. Thanks!

タグ(1)
0 件の賞賛
返信
1 解決策
997件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Just curious as to why you need it. You do not need to populate the 8-bi micro into your final application.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
998件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Just curious as to why you need it. You do not need to populate the 8-bi micro into your final application.

0 件の賞賛
返信
997件の閲覧回数
g_moreno
Contributor III

Hello Fabio,

That is correct, I don't need to include the 8-bit MCU into my final application. The problem is that this MCU has many signals that enable or select specific configurations for several peripherals. If this MCU is removed without the corresponding BSP update, the boot sequence is interrupted waiting for communication with the MCU from different drivers. My main interest is to make the appropriate modifications in the source code depending on the peripherals I use so that the signals of interest are controlled or monitored as they are in the DZ60 MCU.

0 件の賞賛
返信
997件の閲覧回数
hakamo
Contributor I

Hi

Anyone can tell me what is exactly functionality of this MCU and how can i bypass or omit it in final application or is there any document and source code related to this MCU !?

Unfortunately in freescale PDK download page isn't any document about functionality of it !

0 件の賞賛
返信
997件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please look at Chapter 1 (MC9S08DZ60-PMIC Protocol Driver) of "pdk2009_12_mx35_Linux_RM.pdf"
in Linux documentation.

0 件の賞賛
返信