i.MX28 VDD4P2 Regulated Output and Absolute Maximum Rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 VDD4P2 Regulated Output and Absolute Maximum Rating

Jump to solution
1,008 Views
george
Senior Contributor II

Dear all,

We doubt about the description of the following data sheets.

Somebody should tell the correct interpretation.

  • The absolute maximum rationg of VDD4P2

pastedImage_0.png

  • The VDD4P2 output voltage accuracy

pastedImage_3.png

Aren't two parameters described above contradictory?

Best Regards,

George

Labels (1)
Tags (1)
0 Kudos
1 Solution
780 Views
Yuri
NXP Employee
NXP Employee

Really : Maximum DCDC_BATT / BATT / VDD4p2  value is 4.242 V, even including accuracy of 3 % for VDD4p2.


~Yuri.

View solution in original post

0 Kudos
7 Replies
780 Views
Yuri
NXP Employee
NXP Employee

Maximum DCDC_BATT / BATT value is 4.242 V, including accuracy (of 3 %),
mainly – in order to avoid  maximum charging voltage for  the Li-Ion batteries.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

780 Views
Aemj
Contributor IV

Dear Yuri,

Sorry, please let me know a little in more detail.

How meaning are "VDD4P2V" described in the symbol of Table 6 ?

Does it differ from the VDD4P2 internal regulator output?

Best Regards,

George

0 Kudos
780 Views
Yuri
NXP Employee
NXP Employee

  The "VDD4P2V" - described in the symbol of Table 6 - yes, it is VDD4P2 regulator

output, which may be used as input of the internal DCDC converter. In this sense it
should be "close" to DCDC_BAT.

Regards,

Yuri.

780 Views
george
Senior Contributor II

Dear Yuri,

Thank you for the comment.

I have understood the above your comment somehow.

Please let me know a little in more detail only about "Maximum DCDC_BATT / BATT value is 4.242 V, including accuracy (of 3 %)".

The 4.242V seem to be +1%.


BR,

George

0 Kudos
781 Views
Yuri
NXP Employee
NXP Employee

Really : Maximum DCDC_BATT / BATT / VDD4p2  value is 4.242 V, even including accuracy of 3 % for VDD4p2.


~Yuri.

0 Kudos
780 Views
michaelkoelbl
Contributor III

Hello Yuri,

we have an external charger (TI bq24250) which has a SYS-output where it provides a regulated output in case 5V are present. This SYS-output we want to connect do the DCDC_BATT and BATT pins of the iMX28. This voltage is litte greater than the mentioned max value of 4.242V, it can be as much as 4.37V. Is this allowed?

For the sake of completeness: the charger switches the battery voltage to SYS-output as soon as the 5V are gone.

Thanks,

Michael

0 Kudos
780 Views
Yuri
NXP Employee
NXP Employee

Hello,

I am afraid the maximum  value for both DCDC_BATT and BATT is 4.242 V.

This is stated separately for battery charging pin BATT  and for DCDC input

voltage pin (DCDC_BATT) in the Table 6 (DC Absolute Maximum Ratings).
Maximum charging voltage for  the Li-Ion relates to the BATT pin only.

Regards,

Yuri.

0 Kudos