i.MX28 Enet Frame Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX28 Enet Frame Error

ソリューションへジャンプ
2,277件の閲覧回数
hanspetergredig
Contributor I

We are using the TQMa28 Module from TQ-Systems with an i.MX28 processor and Linux 3.4.14. For communicating with the host and other subdevices we use the two ethernet controller "eth0" and "eth1" both in 100 Mbps/Full-duplex mode . On "eth0" everything works fine, but on "eth1" I always get ethernet frame errors when receiving data. Transmitting data over the same interface does not produce any errors. We can ignore these errors, all data received are complete and correct. But I want to know the reason for these frame errors.

The frame errors are shown in the output of the "ifconfig" command:

RX packets:60 errors:60 dropped:0 overruns:0 frame:60

Further analysis with the "ethtool -S eth1" command shows the following:

rx_packets: 60

rx_crc_errors: 0

IEEE_rx_frame_ok: 0

The last one should be 60. This means that Bit 2 [CR] of the Legacy FEC Receive Buffer Descriptor is set (see Table 26-1 in the [i.MX28 Applications Processor Reference Manual, Rev 1, 2010]). Chapter 26.2.2.1.1.13 says that a Rx CRC or Rx Frame error occured, but the ethtool does not show any CRC error. Therefore I believe in a frame error.

My question: what causes the i.MX28 ENET to set this frame error bit?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,048件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Perhaps the issue relates to the following :

when use both Ethernet ports of the i.MX28, and when signal SPDIF

is used as GPIO and pulled up, ENET1 does not work.

This is a design limitation - the SPDIF signal is multiplexed with ENET1_RX_ER and

it is always connected to (internal)  ENET1_RX_ER. As a result,  all ENET1 received

packages are considered as  having CRC error.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,049件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Perhaps the issue relates to the following :

when use both Ethernet ports of the i.MX28, and when signal SPDIF

is used as GPIO and pulled up, ENET1 does not work.

This is a design limitation - the SPDIF signal is multiplexed with ENET1_RX_ER and

it is always connected to (internal)  ENET1_RX_ER. As a result,  all ENET1 received

packages are considered as  having CRC error.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信