i.MX233 Board not powering up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX233 Board not powering up

872件の閲覧回数
GopiNagaBharath
Contributor IV

Hello,

I have a custom board designed based on the i.MX23 CPU. When I powered the Battery input with 3.7V, the VDDXTAL is not giving out 1V. Since the VDDXTAL is source for turning ON the board with PSWITCH, I am unable to get the voltage on any other rails. Since the PMIC is internal and OFF, none of the power supply rails are active.

We have already designed i.MX23 based custom board which was working properly. This is a new design (with small changes from previous version) which is having this issue.

What are the reasons for the VDDXTAL not going to 1V (it is always 0V) ? I have probed the crystals, they too seem to be not powered and there is no clock.

Regards,

Gopi

タグ(1)
0 件の賞賛
返信
2 返答(返信)

740件の閲覧回数
YixingKong
Senior Contributor IV

Gopi Naga

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

740件の閲覧回数
YixingKong
Senior Contributor IV

Gopi Naga

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信