I am trying to build i.MX Yocto and it fails when trying to download the file: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-hantro-daemon-1.1.0.tar.gz
After a while this worked once. It looks like there is an issue on a particular NXP server at IP address 72.246.146.170 and when the selected IP address changed to 23.195.116.74 all was then ok. After that the selected IP address went back to 72.246.146.170 and the build failed.
Looks like someone at NXP needs to fix this ...
wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-hantro-daemon-1.1.0.tar.gz
--2021-11-30 12:35:28-- https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-hantro-daemon-1.1.0.tar.gz?ver=1
Resolving www.nxp.com (www.nxp.com)... 72.246.146.170
Connecting to www.nxp.com (www.nxp.com)|72.246.146.170|:443... connected.
HTTP request sent, awaiting response... 304 Not Modified
2021-11-30 12:35:28 ERROR 304: Not Modified.
[terry@study tmp]$ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-hantro-daemon-1.1.0.tar.gz
--2021-11-30 12:45:12-- https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-hantro-daemon-1.1.0.tar.gz
Resolving www.nxp.com (www.nxp.com)... 23.195.116.74
Connecting to www.nxp.com (www.nxp.com)|23.195.116.74|:443... connected.
HTTP request sent, awaiting response... 200 OK
Length: 129316 (126K) [application/x-gzip]
Saving to: ‘imx-vpu-hantro-daemon-1.1.0.tar.gz’
imx-vpu-hantro-daemon-1.1.0.tar.gz 100%[======================================================================>] 126.29K --.-KB/s in 0.008s
2021-11-30 12:45:12 (15.6 MB/s) - ‘imx-vpu-hantro-daemon-1.1.0.tar.gz’ saved [129316/129316]
I had similar problem when try to build L5.10.72 using bitbake imx-image-multimedia but the problem was "imx-vpu-hantro-daemon-1.1.1.tar.gz" was not able to fetch, not same as original post mention "imx-vpu-hantro-daemon-1.1.0.tar.gz", is there any fix for this problem? Thanks.
I have managed to do this by hard coding the IP address of 104.84.242.171 for www.nxp.com in the systems /etc/hosts file as the host 104.84.242.171 appeared to work and the Yocto build then continued.