I'm designing RT1170 application and planning to use an external oscillator for 24MHz on XTALI instead of a crystal.
Would you tell me the requirements of external oscillator? Frequency stability (ppm), output load, jitter and etc.
解決済! 解決策の投稿を見る。
Hi @Eugene3,
As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.
Let me know if this helps.
BR,
Edwin.
Hi @Eugene3,
As long as the external 24MHz oscillator complies with the description seen in "Table 4. Clocks configurations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor, you will be OK. As you can see, the restrictions mostly depend on whether or not you are using USB and/or Ethernet.
Let me know if this helps.
BR,
Edwin.
Hi @EdwinHz
Thank you, I got it.