Hi All
What the difference in PWM and FlexIO PWM?
II want to use PWM signal to control BLDC motor.
And, in each PWM period I want to do ADC for current sensing.
For this aim, I refer
sample projects, but I don't really know the difference.
Below figure is the modify result of the evkmimxrt1060_pwm. Maybe this can use for BLDC control.
What I would like to know is whether FlexIO PWM is more suitable for controlling BLDC or not?
已解决! 转到解答。
Hello Kenji,
If the microcontroller does have a dedicated FlexPWM module, as it’s the case with the i.MXRT1060, I would recommend using the FlexPWM module to generate the PWM signals.
The examples are similar but the FlexIO examples use the FlexIO modules to generate the PWM waveforms, instead of using the dedicated FlexPWM module.
I hope that this information helps.
Regards,
Gustavo
Hello Kenji,
If the microcontroller does have a dedicated FlexPWM module, as it’s the case with the i.MXRT1060, I would recommend using the FlexPWM module to generate the PWM signals.
The examples are similar but the FlexIO examples use the FlexIO modules to generate the PWM waveforms, instead of using the dedicated FlexPWM module.
I hope that this information helps.
Regards,
Gustavo
The difference and intended use is not clear.
But I think, it's better to use FlexPWM for my aim.
Thank you.