The SEMC interface supports 4 types of devices, I would like to confirm the following questions:
1. Does it support access two different devices through the SEMC interface in the same project, such as an external SDRAM plug-in, an external SRAM, and data interaction with two peripherals is required in the same project.
2. If it is supported, how much delay is there when the two devices are switched?
thankyou!
已解决! 转到解答。