i.MX RT1052 Processor的SEMC接口

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1052 Processor的SEMC接口

ソリューションへジャンプ
1,075件の閲覧回数
jiaxin
Contributor I

The SEMC interface supports 4 types of devices, I would like to confirm the following questions:

1. Does it support access two different devices through the SEMC interface in the same project, such as an external SDRAM plug-in, an external SRAM, and data interaction with two peripherals is required in the same project.

2. If it is supported, how much delay is there when the two devices are switched?

thankyou!

0 件の賞賛
返信
1 解決策
1,040件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @jiaxin ,

1. Yes, 可以支持。他们的CS是不同的。数据线可能是复用的。

2. 这个很难讲。从一个cs起来到另一个落下大概需要3~4个clock。

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,041件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @jiaxin ,

1. Yes, 可以支持。他们的CS是不同的。数据线可能是复用的。

2. 这个很难讲。从一个cs起来到另一个落下大概需要3~4个clock。

 

Regards,

Jing

0 件の賞賛
返信
1,051件の閲覧回数
jiaxin
Contributor I

Hi,NXP

      Is there anyone who know answer?

0 件の賞賛
返信