Hi @hiro33
1. When you enter the serial download mode, do you use USB HID or UART to download the code?
If you are using the USB HID, can you find the PID VID?
Then, can you connect the chip or not?
Do you use the Secure provisional tool or the MCUbootUtility to download the code?
2. Do you use external debugger? Can you download the code to the internal RAM through the SWD?
3. What's the external flash you are using, if QSPI, you need to enable the QE bit to the new chip.
Best Regrads
Kerry