i.MX 93 ADC Hardware Triggers Combined GPIO interrupt.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 93 ADC Hardware Triggers Combined GPIO interrupt.

Jump to solution
388 Views
NZP
Contributor III

Hello Experts,

I want to read I.MX 93 ADC CH0 using hardware trigger (Rising Edge) of GPIO1's pin GPIO1.IO[0] but after reading RM of imx93 I got below details.

72.1.2 Hardware Triggers

NZP_0-1709704981103.png

So, my question is that,

1. Combined interrupt indication for all GPIO1 signal means:  will my ADC CH0 trigger when Rising Edge comes on any interrupt configured PIN of GPIO1 port?

Thanks.

0 Kudos
Reply
1 Solution
359 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @NZP 

 

Yes, th IRQ logic in GPIO1 is OR. The IRQ10 will be handled.

Zhiming_Liu_0-1709868029932.png

 

Best Regards

Zhiming

View solution in original post

1 Reply
360 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @NZP 

 

Yes, th IRQ logic in GPIO1 is OR. The IRQ10 will be handled.

Zhiming_Liu_0-1709868029932.png

 

Best Regards

Zhiming