i.MX 8M Plus and RTL8211F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus and RTL8211F

1,487 Views
www1519
Contributor III

Hi NXP Engineer

In my design refer to NXP EVK, imx8m plus + RTL8211F is used.

5 PCBs are producted, and only 1 PCB ‘s network card had problem.

as below, when ifconfig, only lo

but when ifconfig -a ,  eth0 is shown.

The communicaiont is failure for PC and RTL 8211.

the remaining 4 PCBs ,have eth0 when using config not ifconfig -a.

please confirm. Thanks a lot.

www1519_0-1693145132204.png

www1519_1-1693145265893.png

www1519_3-1693146100746.png

Best Regards!

 

0 Kudos
Reply
3 Replies

1,344 Views
www1519
Contributor III

Hi @JosephAtNXP 

As below, confirm pls. thanks.

www1519_0-1693387143642.png

Best Regards!

 

0 Kudos
Reply

1,314 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi @www1519,

I assume that your five boards are exactly the same schematic with exactly same part number for every component, am I right?

Seems that PHY is not responding maybe in time or speed, could you scope that the PHY is properly clock-fed and the MDIO lines actually have both-side communication?

Also, check for bootstrapping settings, did you populate the same bootstrap resistors?

Thank you

0 Kudos
Reply

1,365 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Does the PHY still fail when you run this command?

$ ifconfig eth0 up

The IF hasn't the UP flag, that's why it doesn't appear on ifconfig output.

The ping will fail until it has an IP and a RUNNING flag.

Regards

0 Kudos
Reply