i.MX 8M Plus Manual Description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus Manual Description

Jump to solution
1,185 Views
www1519
Contributor III

Hi! NXP Engineer

Is Ground*RX_P/N = "RX_P and RX_N pins are connected to Ground" in  i.MX 8M Plus Hardware Developer’s Guide?

Thanks a lot

www1519_1-1680769703066.png

 

The same as above  in i.MX 8M Plus Applications Processor Datasheet for Consumer Products.

 

www1519_0-1680769645496.png

 

0 Kudos
Reply
1 Solution
1,127 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @www1519,

Unused signal termination is recommended to follow for:

1. Noise immunity
2. To reduce additional power consumption.

Thanks & Regards,
Ritesh M Patel

View solution in original post

0 Kudos
Reply
6 Replies
1,162 Views
www1519
Contributor III

Hi Mr.Ritesh M Patel@riteshmpatel 

I see. Thank you.

But according to ds, if USB1 or USB2 or USB1&2 do not used, USBx_RX_P and USBx_RX_N should be connected to the Ground.

If USB1 & USB2 are used as USB 2.0(not USB 3.0), USBx_RX_P and USBx_RX_N should be connected to the Ground? or be floating?

(I think USBx_RX_P and USBx_RX_N are used for USB 3.0)

0 Kudos
Reply
1,159 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @www1519,

If USB 2.0 connections are only used, USBx_RX_P and USBx_RX_N should be connected to the Ground.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply
1,155 Views
www1519
Contributor III

Hi Mr.Ritesh M Patel @riteshmpatel 

Thank you for your reply.

>If USB 2.0 connections are only used, USBx_RX_P and USBx_RX_N should be connected to the Ground.

→I see.Thank you.

    If They are not connected to the GND, and only  power consumption of SoC is increasing, is correct?

 

0 Kudos
Reply
1,128 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @www1519,

Unused signal termination is recommended to follow for:

1. Noise immunity
2. To reduce additional power consumption.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply
1,051 Views
www1519
Contributor III
Hi Mr.Ritesh M Patel @riteshmpatel

Thank you for your reply.
0 Kudos
Reply
1,170 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @www1519,

I hope you are doing well.

If USBx_RX_P and USBx_RX_N are not used, they should be connected to the Ground.

Thanks & Regards,
Ritesh M Patel

 

0 Kudos
Reply