i.MX 8M Plus FlexCAN running while CPU cores suspended

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8M Plus FlexCAN running while CPU cores suspended

662 次查看
matbus
Contributor II

On i.MX 8M Plus, can the FlexCAN be alive while the CPU cores are suspended? With
hardware filters we can then have the FlexCAN interrupt the CPU on
specific frames and deliver them. I mean have the CAN controller and CAN
tranceiver fully running at some power consumption cost?

0 项奖励
回复
3 回复数

653 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mattias

 

for such case one can look at sect.11.8.2.1.1.4 Stop mode 

i.MX 8M Plus Applications Processor Reference Manual

 

Best regards
igor

646 次查看
matbus
Contributor II

Hi Igor,

 

Thanks for the reply. However, the FlexCAN cannot wake up on a specific frame here as I understand or am I wrong? We need to wake up on a normal CAN frame.

0 项奖励
回复

641 次查看
igorpadykov
NXP Employee
NXP Employee

one can try to leave FlexCAN running in low power mode configuring its CCM_CCGR53,54 registers,

clock gate control is described in sect. 5.1.7.6 CCM Clock Gating Register (CCM_CCGRn)  i.MX 8M Plus Applications Processor Reference Manual

 

Best regards
igor

 

 

 

 

 

0 项奖励
回复