i.MX 8M Nano EVK - GUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Nano EVK - GUI

1,154件の閲覧回数
OliverT
Contributor I

Hello,

We were trying to setup a i.MX 8M Nano EVK Board with a graphical user interface. Our goal is to first have some kind of Desktop OS, like Gnome, and then compile/execute some applications with GUI.

Our first step was to build the core-image-sato with yocto.
Loading it into the board seems to be no problem, but when we boot the board and check the HDMI output we only get a shell.

When we try to manually start Xserver with startx we receive an error "Cannot run in framebuffer mode. Please specify busIDs for all framebuffer devices" (See console_output.txt)

In /var/log/Xorg.0.log we see extended error.

We tried to let Xserver auto configure the board with  Xorg -configure but this fails as well (Xorg-configure.txt)

Now we are stumped. We already tried resolving this on our own, but to no avail. According to Google we seem to be the only ones trying to setup a GUI on this board. Have we overlooked something?

There MUST be someway to get a GUI working on this board.

We'd be grateful for any help

タグ(3)
0 件の賞賛
1 返信

1,137件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛