Hello
At first, I have success build with `MACHINE=imx8mnddr4ab2 ` but Build failed on the other console as below.
bryanhong@sombra:build$ bitbake core-image-base
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
MACHINE=imx8mnddr4ab2 is invalid. Please set a valid MACHINE in your local.conf, environment or other configuration file.
thanks
bryan
Solved! Go to Solution.
I restart build with new build directory. and then Above MACHINE issue not presented.
I restart build with new build directory. and then Above MACHINE issue not presented.
console 1
I have execute below.
1. repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.24-2.1.0.xml
2. repo sync
3. EULA=1 MACHINE=imx8mnddr4ab2 DISTRO=fsl-imx-xwayland source ./fsl-setup-af.sh -b build
4. bitbake fsl-image-af-littlekernel
and then the build success.
next
I have lunch console 2. and execute below
console 2
1. EULA=1 MACHINE=imx8mnddr4ab2 DISTRO=fsl-imx-xwayland source ./fsl-setup-af.sh -b build
2. bitbake fsl-image-af-littlekernel <-- ERROR
you built completely in console 1 and built successfully, then close the console 1 and open console 2, enter the same build folder, and use the same build command, but you get the error?
"At first, I have success build with `MACHINE=imx8mnddr4ab2 ` but Build failed on the other console as below."
>what do you mean? which console you build successfully, and which console you build failed?