i.MX 8M Mini EVK : Burn the NXP Linux BSP image to the board fail-- Need help

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8M Mini EVK : Burn the NXP Linux BSP image to the board fail-- Need help

598 次查看
YC_Hor
Contributor I

Hi,

I follow the web guideline to flash the embedded Linux into iMX 8M Mini board,

(https://www.nxp.com/document/guide/get-started-with-the-i-mx-8m-mini-evk:GS-iMX-8M-Mini-EVK)

When execute the uuu command to flash the Linux BSP zip image file, the Step stop at the 3:3 1/ 1 (as below) and can not continue next step , and also no "done or success" display.

Can you give some advisement how to solve ?

 

------------------------------------CMD-------------------------------------------------------

sudo ./uuu LF_v5.10_1.0.0_images_IMX8MMEVK.zip
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.127-0-g08c58c9

Success 0 Failure 0

Prep 1/ 0 [=================100%=================] Http Download\Uncompress
3:3 1/ 1 [=================100%=================] mx8mmevk-sd.bin-flash_evk

 

-----------------------------------System--------------------------------------------------

O/S : ubuntu 18.04

Board: NXP i.MX 8M Mini LPDDR4 EVKB board

uuu version: 1.4.127

Linux BSP: L5.10.9_1.0.0_MX8MM

 

0 项奖励
回复
1 回复

589 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yc

 

one can try to follow sect.4.2.2 Using UUU  i.MX Linux User’s Guide​

 

Best regards
igor

0 项奖励
回复