i.MX 8M Family DDR Tool Usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Family DDR Tool Usage

639件の閲覧回数
pantarun_92
Contributor I

i.MX8MSCALE DDR Tool User’s Guide mentions using a USB port for downloading a test
image to the i.MX series processor’s internal RAM through a USB connection for running the DDR stress test via host PC & a UART interface for debugging & logging.

Is it possible to perform Stress test from host PC over UART or JTAG interfaces if one does not have any spare USB interfaces to put on board for external USB connections on the customized board? 

What could be the solution to perform DDR stress test in such an application? Which interface can be used as alternative to USB interface for running DDR stress test?

How will this affect the RPA file? 

0 件の賞賛
返信
3 返答(返信)

635件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ARUN

 

>Is it possible to perform Stress test from host PC over UART or JTAG interfaces if one
>does not have any spare USB interfaces to put on board for external USB connections

>on the customized board?

 

sorry this is not possible.

 

Best regards
igor

0 件の賞賛
返信

633件の閲覧回数
pantarun_92
Contributor I

Igor,

Is it possible to flash eMMC/SD card with UART interface only, if we do not have a dedicated USB type C port as on EVK? external USB interface is must for it too?

0 件の賞賛
返信

627件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

for " flash eMMC/SD" question please create new thread as this is new question.

 

Best regards
igor

0 件の賞賛
返信