i.MX 8M Family DDR Tool Hangs on Waiting for the target board boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Family DDR Tool Hangs on Waiting for the target board boot

Jump to solution
1,727 Views
onurcalili
Contributor I

Hello everyone,

We have designed a custom board with i.MX 8M Quad CPU. We controlled the voltages and clocks on the board. But when we try DDR Tool, it prints the logs given below Tool does not print anything after "Waiting for the target board boot...". We stuck at this point. What can we try after this point? Any help appreciated. 

Downloading file 'bin\lpddr4_train1d_string.bin' ..Done

Downloading file 'bin\lpddr4_train2d_string.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_1d_imem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_1d_dmem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_2d_imem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_2d_dmem.bin' ..Done

Downloading IVT header...Done
Downloading file 'bin\m850_ddr_stress_test.bin' ...Done

Download is complete
Waiting for the target board boot...

Thanks.

Onur

0 Kudos
1 Solution
1,617 Views
igorpadykov
NXP Employee
NXP Employee

Hi Onur

one can check uart, if it is different from reference board add configuration

in script (MX 8M Family DDR Tool link provides examples).

DDR Tool UART Usage 

i.MX 8M Family DDR Tool Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
1,617 Views
onurcalili
Contributor I

Hi Igor, 

Thanks for advice. The problem was in our design. We have an usb to uart converter in our board and its rx tx lines are not crossed on the board. When we corrected the rx and tx lines now i can see the output on DDR Tool.

Best regards

Onur

0 Kudos
1,618 Views
igorpadykov
NXP Employee
NXP Employee

Hi Onur

one can check uart, if it is different from reference board add configuration

in script (MX 8M Family DDR Tool link provides examples).

DDR Tool UART Usage 

i.MX 8M Family DDR Tool Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,617 Views
adevries
Contributor V

I am encountering a similar issue, any help on this would be appreciated

0 Kudos