Hi,
I have waste so much time in search but without success and I hope you can help me by answering my question about ethernet access from Cortex-M4.
Is it possible to use the ethernet interface for example with FreeRTOS on the Cortex-M4?
Is this possible in principial?
For many other processors including the i.MX 7ULP there exists muiltiple useful files for example fsl_clock.c/h, fsl_common.c/h, and <processor>_features.h files. Do they exist also for the i.MX 7Dual processor? If yes, where can i get these files?
The exact processor: MCIMX7D5EVM10SC
Thanks in advance for your reply.
解決済! 解決策の投稿を見る。
Hi Andreas
>Do you know if there are such files for the i.MX 7Dual processor?
sorry I am not aware of such files for FreeRTOS.
I think you should develop them yourself using for example uboot sources.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Andreas
>Is it possible to use the ethernet interface for example with FreeRTOS on the Cortex-M4?
>Is this possible in principial?
yes possible. One can look at 2.1.3 Cortex-M4 Memory Map (AIPS-3, ENET)
i.MX 7Dual Applications Processor Reference Manua
Access permissions may be configured with RDC described in sect.3.2
Resource Domain Controller (RDC)
Uboot enet example can be reused for porting to FreeRTOS
mx7dsabresd.c\mx7dsabresd\freescale\board - uboot-imx - i.MX U-Boot
fec_mxc.c\net\drivers - uboot-imx - i.MX U-Boot
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
thank you for the quick and useful answer.
>For many other processors including the i.MX 7ULP there exists muiltiple useful files for example fsl_clock.c/h, fsl_common.c/h, and <processor>_features.h files. Do they exist also for the i.MX 7Dual processor? If yes, where can i get these files?
Do you know if there are such files for the i.MX 7Dual processor?
Best regards,
Andreas
Hi Andreas
>Do you know if there are such files for the i.MX 7Dual processor?
sorry I am not aware of such files for FreeRTOS.
I think you should develop them yourself using for example uboot sources.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------