"Demo Images - SABRE Board based on i.MX 7 Dual" has u-boot / boot / recovery epdc version, but what is different?
How can I build the epdc version?
I will transfer it to a different EPD for IMXEBOOKDC4.
And fix mxc_epdc_fb.c.
How do you build an epd version?
Hi hiroyuki
please include epdc driver as described in Chapter 10 Electrophoretic Display Controller
(EPDC) Frame Buffer Driver attached Linux Manual and use
Table 10. Common kernel boot parameters attached Release Notes
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I saw Chapter 10 of the i.MX Linux® Reference Manual.
However, we did not need to change anything except support for splash screen.
Enable below
#define CONFIG_SPLASH_SCREEN
#define CONFIG_MXC_EPDC
Is the epdc version of "Demo Images - SABRE Board based on i.MX 7 Dual" supporting splash screen support?
Moreover, I do not understand the following method.
10.3.7 Enabling an EPDC Splash Screen
3. Write the firmware file to the SD card at the FAT partition.
cp epdc_E060SCM.bin [FAT partition on SD card]
The following is the partition of the SD card.
Where can I make a FAT partition and copy it?
Create a new partition with sdb13 with FAT,
Is it OK with the operation below?
> sudo mount/dev/sdb13/mnt
> sudo cp epdc_E060SCM_splash.bin /mnt/epdc_E060SCM.bin
> sudo umount /mnt