Hi, I wired OV5640 camera to the CSI0 interface of the i.MX 6Quad Sabrelite board, the os is android 4.0.4,kernel is 3.0.15.
After I ran the camera application, it displayed black screen and got some error like below:
/*******************************************************************/
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
/*******************************************************************/
The I2C communication is ok, because the ov5640 driver could read the id of the ov5640 chip:
/*******************************************************************/
<<-OV5640-DEBUG->>[1531]ov5640 Model ID 0x5640, Revision 0xb0
/*******************************************************************/
I used oscilloscope to detect the signals of hardware, and it seemed no problem:
1)the MCLK pin outputs 24M waveform
2)the HSYNC, VSYNC output square wave
3) CSI0_DAT12~CSI0_DAT19 output waveform
the file for ov5640 driver is drivers/media/video/mxc/capture/ov5640.c, i only made some change in probe() function for porting:
const struct i2c_device_id *id)
{
...
ov5640_data.csi = plat_data->csi; //csi0
ov5640_data.io_init = plat_data->io_init; //see board-mx6q_sabrelite.c
ov5640_data.i2c_client = client;
ov5640_data.pix.pixelformat = V4L2_PIX_FMT_YUYV; //choose output format
ov5640_data.pix.width = 1280;//640; //set the width 1280
ov5640_data.pix.height = 760;//480; //set the height 760
ov5640_data.streamcap.capability = V4L2_MODE_HIGHQUALITY |
V4L2_CAP_TIMEPERFRAME;
ov5640_data.streamcap.capturemode = 4;//0; //set mode ov5640_mode_720P_1280_720
...
}
the io_init refers to the function mx6q_csi0_io_ini of board-mx6q_sabrelite.c:
{
...
gpio_request(MX6Q_SABRELITE_CAM2_RST, "cam2-reset");
gpio_direction_output(MX6Q_SABRELITE_CAM2_RST, 0);
gpio_request(MX6Q_SABRELITE_CAM2_PWN, "cam2-pwdn");
gpio_direction_output(MX6Q_SABRELITE_CAM2_PWN, 1);
msleep(5);
gpio_set_value(MX6Q_SABRELITE_CAM2_PWN, 0);
msleep(1);
gpio_set_value(MX6Q_SABRELITE_CAM2_RST, 1);
}
can anyone know how to fix this problem ?
ov5640_data.pix.height = 760;//480; //set the height 760
ov5640_data.streamcap.capturemode = 4;//0; //set mode ov5640_mode_720P_1280_720
760?
Same problem with ov5640_mipi camera, and kernel 3.0.35.
If the capturemode is set to 255 in: hardware/imx/mx6/libcamera/V4l2CsiDevice.cpp, a green screen appears with the 'Camera' app, and the error is gone but no image. If any other capturemode is forced the error still.