Hi,
Im currently running Kernel 3.14.28-1.0.0-ga (from the freescale git repository) with a few patches and have issues with resume that look a lot like what ERR005723 related documents describe. Without any additional output, I can see the hang after the "CPU1 is up" output during resume. Once I "disabled" PCI in my device tree, resume works fine.
In my hardware design, one Cyclone V Altera FPGA is connected to a "Keith & Koep Trizeps VII".
In the git repository (334af1b0) and in the code I can see that the "not official" fix using the PHY-power-down in GPR1 is part of the kernel. However, the system hangs when it tries to get the FPGA out of the D3 power state and before my driver is called (in pci_raw_set_power_state from drivers/pci/pci.h). This whole hang is made complicated by the fact that when I start adding printk and similar outputs, the behavior changes until with enough output (using the serial console, so it's slow) the system resumes successfully.
Here is a couple of things I tried:
The second one is a bit strange, as the FPGA currently only supports gen1.
I'm trying to get a hold of this and would like to avoid adding some random printks and the delays it brings just because "it fixes stuff" (or not: System will not resume from suspend to memory with PCIE enabled). Any help would be greatly appreciated.
Cheers
Kai
Hi Kai
one can look at ERR005723 patches below
SW workarounds used to fix ERR005723 in Linux BSP(private)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I know that page already.
As mentioned, the GRP1 based patch is already applied to 3.14.28 (albeit directly in pci-imx6.c).
The second method of warm-resetting the PHY is only implemented for 3.0.35 and isn't even close to applying to 3.14.28.