i.MX 6Dual burning failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6Dual burning failed

978 Views
li_hong
Contributor III

Hello,Team:

      I'm using fsl-imx6 board with i.MX 6Dual Processor,and i download the demo binary form L4.14.78_1.0.0_MX6QDLSOLOX .I try to burn with the downloaded binary(fsl-image-validation-imx-imx6qpdlsolox.sdcard and u-boot-imx6dlsabresd_sd.imx),but the process abort after a while.

      In addition,I've not found out imx6dsabresd.conf but imx6dlsabresd.conf in machine directory.what's difference between  imx6dsabresd and imx6dlsabresd.

 Thank you.

Labels (1)
3 Replies

841 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

I see by the image you share that you are using UUU to flash your board,

Could you share the script that you're using (UUU.auto)?

 

In your case you'll need to rename the uuu.auto-imx6dlsabresd to uuu.auto, place it inside the zip file and run the command:

.\uuu.exe L4.14.78_1.0.0_ga_images_MX6QPDLSOLOX.zip

This will burn the yocto image to the eMMC

 

Hope this helps,

Best regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

841 Views
li_hong
Contributor III

Hello,

I try to  change the u-boot image (from u-boot-imx6dlsabresd_sd.imx to u-boot-imx6qsabresd_sd.imx) ,and sloven this problem.

Thank you.

841 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for sharing how you solved this with everyone,

 

Best regards,

Aldo.

0 Kudos
Reply