i.MX 6Dual/6Quad HDMI and VGA can not read edid data with i2c.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 6Dual/6Quad HDMI and VGA can not read edid data with i2c.

520 次查看
zhengguang_yang
Contributor II

Linux:3.14.28

The default EDID is from the device tree.Whether 3.14.28 linux does not support the acquisition of EDID from I2C

标记 (2)
0 项奖励
1 回复

408 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

it is working fine with nxp official linux releases

i.MX 6 Series Software and Development Tool|NXP 

please check if proper HDMI cable used, check that you use "true"

HDMI or just a HDMI - DVI adapter.
"True" HDMI display with special HDMI cable should be used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励