i.MX 1062: s there any sample code for sensorless trapezoidal control of BLDC motor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 1062: s there any sample code for sensorless trapezoidal control of BLDC motor

909件の閲覧回数
kenji
Contributor IV

Hi All

Is there any sample code for sensorless trapezoidal control of BLDC motor, using i.MX processors?

I want to know how to set the 6CH of FlexPWM output only.
I'm not interested in the control method.

This is the PWM output pattern in STM32 MCU I made, and I would like to know how to set in i.MX MCUs to obtain the same output.

 

kenji_0-1626773967576.png

 

 
タグ(1)
0 件の賞賛
返信
1 返信

901件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Kenji,

I would recommend you to start from the PWM examples we have in our MCUXpresso SDK, once you are familiar with the examples you can modify them according to your needs. If you have any specific question please do not hesitate to let us know.

You can download RT1062 SDK from the next link: Welcome | MCUXpresso SDK Builder

Best regards,

Felipe

0 件の賞賛
返信