how to setup GPMI NAND timing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to setup GPMI NAND timing

跳至解决方案
2,185 次查看
x10
Contributor V

Hi, all

In Linux gpmi nand driver for imx28evk, I can not find the code to setup timing parameters into hardware registers. For example, in gpmi-nfc-hal-v1.c, the funtion set_timing(...) doesn't really write nfc's hardware registers, the function is as follows: 

/**
* set_timing() - Configures the NFC timing.
*
* @this: Per-device data.
* @timing: The timing of interest.
*/
static int set_timing(struct gpmi_nfc_data *this,
const struct gpmi_nfc_timing *timing)
{
struct nfc_hal *nfc = this->nfc;

/* Accept the new timing. */

nfc->timing = *timing;

/* Return success. */

return 0;

}

Some helps are needed for me to figure this problem out. Thanks very much.

BR

Cheng Shi

Emtronix

标签 (1)
0 项奖励
回复
1 解答
1,169 次查看
HuangShijie
Contributor III

yes.

But if the EDO mode is enabled with the ONFI nand.

The timing setting will be changed.

You can read the latest Linus's kernel for reference.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,169 次查看
x10
Contributor V

I'm sure that no real NAND timing setup is done in gpmi_nfc_hal_v1.c. As there are default settings which can work on most of Nandflash chips, all the nandflash r/w work ok.

0 项奖励
回复
1,170 次查看
HuangShijie
Contributor III

yes.

But if the EDO mode is enabled with the ONFI nand.

The timing setting will be changed.

You can read the latest Linus's kernel for reference.

0 项奖励
回复