Hello,
When I run test application it executes fine.
Here is the client side log
#optee_example_hello_world
Invoking TA to increment 42
TA incremented value to 43
Can someone tell me how I can see TA or SW side log?
I the Makefile of hello_world TA, I can see below lines
CFG_TEE_TA_LOG_LEVEL ?= 4
CPPFLAGS += -DCFG_TEE_TA_LOG_LEVEL=$(CFG_TEE_TA_LOG_LEVEL)
The value is 4 means highest verbose for OPTEE log and TA log should be found.
I have read OPTEE documentation. I have connected with a serial port to IMX7. When I run Trutstzone Sample applications from IMX7 serial interface, I can see only CA side log. TA side log does not show.
SO, I have checked flags which have correct values according to OPTEE documentation.
Still the log of TA/Trustzone application is not shown on Serial console.
Do you have any idea ?