hello everyone.
I use OS the Ubuntu 14.04 LTS and i.MX6QLite and I studying website
Build Linux System for IMX6Q Sabre Lite - Linuxpedia
When I typing this sentence
blah blah blah...
make arm=ARM CROSS_COMPILE=arm-linux-gnueabihf- mx6qsabrelite
appear error.
Error message is
'make: *** No rule to make target `mx6q_sabre_lite'. Stop.'
So I used
$ make mrproper and $ make menucinfig
Nevertheless not solve this error
(Path is /home/linux)
How to solve this error?
kong king
Solved! Go to Solution.
Kong,
What is the path to your arm-linux-gnueabihf-gcc ? I typically place it into /opt on my host machine for cross compiling U-boot and the Linux Kernel. If you are using the Linaro toolchain then your path would be something like:
/opt/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/
If this is the case (or wherever you may have placed the toolchain), then you should try:
make ARCH=arm CROSS_COMPILE=<full path to toolchain>/bin/arm-linux-gnueabihf- mx6qsabrelite_defconfig
It may be that you only need mx6qsabrelite and can leave off the _defconfig but I am uncertain about this. Alternatively you can use menuconfig to setup the Kernel/U-boot.
Basically, if you have not modified your host environment variable PATH to include the full path to the arm-linux-gnueabihf-gcc binaries then you just need to declare the full path as the CROSS_COMPILE environment variable. libstdc++.so and libstdc++.so.6 are found under <full path to toolchain>/lib directory
Let me know if this helps,
John
I am hoping it is just a typo but it should be ARCH=arm, correct?
It would be very appreciated.
I try to this sentence..
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- distclean
arm-linux-gnueabihf-gcc: error while loading shared libraries: libstdc++.so.6: cannot open shared object file: No such file or directory
arm-linux-gnueabihf-gcc: error while loading shared libraries: libstdc++.so.6: cannot open shared object file: No such file or directory
dirname: missing operand
Try 'dirname --help' for more information.
lite@ubuntu:~/u-boot$ make ARCH=ARM CROSS_COMPILE=arm-linux-gnueabihf- distclean
arm-linux-gnueabihf-gcc: error while loading shared libraries: libstdc++.so.6: cannot open shared object file: No such file or directory
arm-linux-gnueabihf-gcc: error while loading shared libraries: libstdc++.so.6: cannot open shared object file: No such file or directory
dirname: missing operand
Try 'dirname --help' for more information.
CLEAN scripts/basic
CLEAN scripts/kconfig
CLEAN include/config include/generated
lite@ubuntu:~/u-boot$
lite@ubuntu:~/u-boot$ make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- mx6qsabrelite
arm-linux-gnueabihf-gcc: error while loading shared libraries: libstdc++.so.6: cannot open shared object file: No such file or directory
arm-linux-gnueabihf-gcc: error while loading shared libraries: libstdc++.so.6: cannot open shared object file: No such file or directory
dirname: missing operand
Try 'dirname --help' for more information.
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
SHIPPED scripts/kconfig/zconf.tab.c
SHIPPED scripts/kconfig/zconf.lex.c
SHIPPED scripts/kconfig/zconf.hash.c
HOSTCC scripts/kconfig/zconf.tab.o
HOSTLD scripts/kconfig/conf
scripts/kconfig/conf --silentoldconfig Kconfig
***
*** Configuration file ".config" not found!
***
*** Please run some configurator (e.g. "make oldconfig" or
*** "make menuconfig" or "make xconfig").
***
make[2]: *** [silentoldconfig] Error 1
make[1]: *** [silentoldconfig] Error 2
make: *** No rule to make target `mx6qsabrelite'. Stop.
I don't understand. Sorry.
kong king.
Kong,
What is the path to your arm-linux-gnueabihf-gcc ? I typically place it into /opt on my host machine for cross compiling U-boot and the Linux Kernel. If you are using the Linaro toolchain then your path would be something like:
/opt/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/
If this is the case (or wherever you may have placed the toolchain), then you should try:
make ARCH=arm CROSS_COMPILE=<full path to toolchain>/bin/arm-linux-gnueabihf- mx6qsabrelite_defconfig
It may be that you only need mx6qsabrelite and can leave off the _defconfig but I am uncertain about this. Alternatively you can use menuconfig to setup the Kernel/U-boot.
Basically, if you have not modified your host environment variable PATH to include the full path to the arm-linux-gnueabihf-gcc binaries then you just need to declare the full path as the CROSS_COMPILE environment variable. libstdc++.so and libstdc++.so.6 are found under <full path to toolchain>/lib directory
Let me know if this helps,
John
I check the opt directory.
there were empty..:smileysilly:
So I've followed your advice.:smileyhappy:
The following results came out.
# configuration written to .config
Thank you for your help.:smileylaugh:
Can I ask one more?
I enter the following sentence
sudo apt-get install uboot-mkimage
...blah blah blah
However the following packages replace it:
u-boot-tools:i386 u-boot-tools
...blah blah blah
E: Unable to locate package uboot-i386
...
...
..
I do not understand.:smileyblush:
(I'm english Starter)
What do I need to install?
thank you.
Kong,
If the configuration was written, that's okay. But did U-Boot cross compile for you? I am assuming it completed in success? Try to build the entire thing like so:
[host command line]$ make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- distclean
[host command line]$ make ARCH =arm CROSS_COMPILE=arm-linux-gnueabihf- mx6qsabrelite_config
[host command line]$ make ARCH =arm CROSS_COMPILE=arm-linux-gnueabihf-
If the last command doesn't execute and finish then I still think you need to have the full path to the cross compiler you are using. The menuconfig option is a way to go through and configure the u-boot through a selection menu.
==========
If sudo apt-get install uboot-mkimage isn't downloading: Have you run sudo apt-get update? It may be that the package isn't found because you are pointed at a bad repository.
Alternatively, you can go to: Ubuntu – Details of package u-boot-tools in trusty and download the i386 deb package yourself. Then in the same directory where you downloaded the deb package you can run sudo apt-get install u-boot-tools_2013.10-3_i386.deb which will locally install the u-boot-tools in that deb package. This will include mkimage.
Hope this helps,
John
Hi,
Can you try this:
make arm=ARM CROSS_COMPILE=arm-linux-gnueabihf- mx6qsabrelite_defconfig
Regards,
Alejandro
Oh, thank you very very much! thanks for answer!
Kong king