hello all:
how to get the boot mode from the system registers?
i want to use it to change the command line correctly in boot_stream, thank you!
解決済! 解決策の投稿を見る。
I add your code to boot_prep and I can see the correct result as well.
diff --git a/init-mx28.c b/init-mx28.c
index 26744e0..146477b 100644
--- a/init-mx28.c
+++ b/init-mx28.c
@@ -1422,6 +1422,21 @@ int _start(int arg)
}
printf("finish simple test\r\n");
#endif
+
+#if 1
+ BW_PINCTRL_MUXSEL2_BANK1_PIN00(3);
+ BW_PINCTRL_MUXSEL2_BANK1_PIN01(3);
+ BW_PINCTRL_MUXSEL2_BANK1_PIN02(3);
+ BW_PINCTRL_MUXSEL2_BANK1_PIN03(3);
+ HW_PINCTRL_DOE1_CLR(0X0f);
+ value = HW_PINCTRL_MUXSEL2_RD();
+ printf("HW_PINCTRL_MUXSEL2 = 0x%x\r\n", value);
+ value = HW_PINCTRL_DOE1_RD();
+ printf("HW_PINCTRL_DOE1 = 0x%x\r\n", value);
+ value = HW_PINCTRL_DIN1_RD();
+ printf("HW_PINCTRL_DIN1_RD = 0x%x\r\n", value);
+ printf("Boot Mode = 0x%x\r\n", (value & 0xff));
+#endif
return 0;
}
============================================
HW_PINCTRL_MUXSEL2 = 0xFFFFFFFF
HW_PINCTRL_DOE1 = 0x00000000
HW_PINCTRL_DIN1_RD = 0x04000009
Boot Mode = 0x00000009
by the way:
in boot stream source, i add the follow code:
value = HW_OCOTP_ROMn_RD(0);
printf("HW_OCOTP_ROM0 = 0x%x\r\n", value);
when power on, it print all zeros. what's wrong?
You have to follow the Software Read Sequence describe in i.MX28 reference manual, Chapter 20 to read HW_OCOTP registers. Sample code can be found at drivers/char/fsl_otp.c.
thank you PeterChan
we config the kernel FSL_OTP, and run it , but the value is not match as sd boot mode.
HW_OCOTP_ROM0 read test result as follows:
pwd
/sys/fsl_otp
# ls
HW_OCOTP_CRYPTO0 HW_OCOTP_HWCAP1 HW_OCOTP_ROM0 HW_OCOTP_SRK2
HW_OCOTP_CRYPTO1 HW_OCOTP_HWCAP2 HW_OCOTP_ROM1 HW_OCOTP_SRK3
HW_OCOTP_CRYPTO2 HW_OCOTP_HWCAP3 HW_OCOTP_ROM2 HW_OCOTP_SRK4
HW_OCOTP_CRYPTO3 HW_OCOTP_HWCAP4 HW_OCOTP_ROM3 HW_OCOTP_SRK5
HW_OCOTP_CUST0 HW_OCOTP_HWCAP5 HW_OCOTP_ROM4 HW_OCOTP_SRK6
HW_OCOTP_CUST1 HW_OCOTP_LOCK HW_OCOTP_ROM5 HW_OCOTP_SRK7
HW_OCOTP_CUST2 HW_OCOTP_OPS0 HW_OCOTP_ROM6 HW_OCOTP_SWCAP
HW_OCOTP_CUST3 HW_OCOTP_OPS1 HW_OCOTP_ROM7 HW_OCOTP_UN0
HW_OCOTP_CUSTCAP HW_OCOTP_OPS2 HW_OCOTP_SRK0 HW_OCOTP_UN1
HW_OCOTP_HWCAP0 HW_OCOTP_OPS3 HW_OCOTP_SRK1 HW_OCOTP_UN2
# cat HW_OCOTP_ROM0
0x0
Have you blown the OTP fuse for SD boot? By default, HW_OCOTP_ROM0 is 0. You can use BitBurner.exe to double check this.
If ENABLE_PIN_BOOT_CHECK OTP is not blown, the boot ROM will check LCD_D[4:0] regardless of the state of LCD_RS pin. If ENABLE_PIN_BOOT_CHECK OTP bit is blown, the boot ROM will check the state of LCD_RS pin to determine which option is used.
On i.MX28 EVK, ENABLE_PIN_BOOT_CHECK OTP is not blown and the boot ROM check the LCD_D[4:0] for boot mode.
If you need to read the boot mode from program, you need to configure these LCD pins as GPIO inputs and then read their GPIO input values. Please refer to i.MX28 Reference Manual Chapter 12 "Boot Modes" for more information.
hello PeterChan:
on imx28, we config the h LCD pins as GPIO inputs and then read their GPIO input values, it stiil didn't match the boot mode
the code as follows:
BW_PINCTRL_MUXSEL2_BANK1_PIN00(3);
BW_PINCTRL_MUXSEL2_BANK1_PIN01(3);
BW_PINCTRL_MUXSEL2_BANK1_PIN02(3);
BW_PINCTRL_MUXSEL2_BANK1_PIN03(3);
HW_PINCTRL_DOE1_CLR(0X0f);
value = HW_PINCTRL_DIN1_RD();
printf("HW_PINCTRL_DIN1_RD = 0x%x\r\n", value);
printf("Boot Mode = 0x%x\r\n", (value & 0xff));
1. in sd boot mode, it printed :
HW_PINCTRL_DIN1_RD = 0x0F000001
Boot Mode = 0x00000001
the correct boot mode should be 0X09 (0b1001), Is right ?
2. in nand boot mode , it printed :
HW_PINCTRL_DIN1_RD = 0x0F000000
Boot Mode = 0x00000000
the correct boot mode should be 0X04 (0b0100)
what's wrong ?
I read the boot mode in kernel using the memtool and I can read it successfully.
root@freescale /unit_tests$ ./memtool 0x80018120 1
Reading 0x1 count starting at address 0x80018120
0x80018120: 00000000
root@freescale /unit_tests$ ./memtool 0x80018120=0xff
Writing 32-bit value 0xFF to address 0x80018120
root@freescale /unit_tests$ ./memtool 0x80018120 1
Reading 0x1 count starting at address 0x80018120
0x80018120: 000000FF
root@freescale /unit_tests$ ./memtool 0x80018b10 1
Reading 0x1 count starting at address 0x80018B10
0x80018B10: 00000000
boot mode = 0x9
root@freescale /unit_tests$ ./memtool 0x80018910 1
Reading 0x1 count starting at address 0x80018910
0x80018910: 0B000009
boot mode = 0x4
root@freescale /unit_tests$ ./memtool 0x80018910 1
Reading 0x1 count starting at address 0x80018910
0x80018910: 0F000004
Could you please double check the register values HW_PINCTRL_MUXSEL2 & HW_PINCTRL_DOE1?
I add your code to boot_prep and I can see the correct result as well.
diff --git a/init-mx28.c b/init-mx28.c
index 26744e0..146477b 100644
--- a/init-mx28.c
+++ b/init-mx28.c
@@ -1422,6 +1422,21 @@ int _start(int arg)
}
printf("finish simple test\r\n");
#endif
+
+#if 1
+ BW_PINCTRL_MUXSEL2_BANK1_PIN00(3);
+ BW_PINCTRL_MUXSEL2_BANK1_PIN01(3);
+ BW_PINCTRL_MUXSEL2_BANK1_PIN02(3);
+ BW_PINCTRL_MUXSEL2_BANK1_PIN03(3);
+ HW_PINCTRL_DOE1_CLR(0X0f);
+ value = HW_PINCTRL_MUXSEL2_RD();
+ printf("HW_PINCTRL_MUXSEL2 = 0x%x\r\n", value);
+ value = HW_PINCTRL_DOE1_RD();
+ printf("HW_PINCTRL_DOE1 = 0x%x\r\n", value);
+ value = HW_PINCTRL_DIN1_RD();
+ printf("HW_PINCTRL_DIN1_RD = 0x%x\r\n", value);
+ printf("Boot Mode = 0x%x\r\n", (value & 0xff));
+#endif
return 0;
}
============================================
HW_PINCTRL_MUXSEL2 = 0xFFFFFFFF
HW_PINCTRL_DOE1 = 0x00000000
HW_PINCTRL_DIN1_RD = 0x04000009
Boot Mode = 0x00000009
thank you very much,
we add "deley (10000);" before "value = HW_PINCTRL_DIN1_RD(); " , then we can get the correct result too.
why can't the gpio configuration change immediatlly ?
Probably due to the weak external pull up resistors at the boot pin.