how to fuse yocto images to i.mx6 emmc with uuu?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to fuse yocto images to i.mx6 emmc with uuu?

772 Views
gufengzi
Contributor III

many images are generated after compiling i.mx6 yocto projuect.

how to use the following different rootfs images?

how to use UUU to fuse u-boot/zimage/rootfs to eMMC?

which rootfs file shoud be used?

imx-image-full.env
imx-image-full-imx6qpsabresd-20240108113535.rootfs.manifest
imx-image-full-imx6qpsabresd-20240108113535.rootfs.tar.zst
imx-image-full-imx6qpsabresd-20240108113535.rootfs.wic.bmap
imx-image-full-imx6qpsabresd-20240108113535.rootfs.wic.zst
imx-image-full-imx6qpsabresd-20240108113535.testdata.json
imx-image-full-imx-uboot-bootpart.wks
modules--6.1.36+git0+04b05c5527-r0-imx6qpsabresd-20240104030808.tgz
0 Kudos
Reply
4 Replies

757 Views
Harvey021
NXP TechSupport
NXP TechSupport

You can download the uuu document and tools from: Release Release uuu_1.5.165 · nxp-imx/mfgtools · GitHub

or refer to <4.2 Universal update utility> in Linux User guide. https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

Command for your reference:  uuu -b emmc_all <bootloader> <rootfs.wic.zst/*> 

rootfs: imx-image-full-imx6qpsabresd-20240108113535.rootfs.wic.zst

 

Regards

Harvey

0 Kudos
Reply

754 Views
gufengzi
Contributor III

I can find nothing about dtb version with command  uuu -b emmc_all <bootloader> <rootfs.wic.zst/*> .

which dtb is used?

0 Kudos
Reply

746 Views
Harvey021
NXP TechSupport
NXP TechSupport

I don't have the Yocto one but should be one as imx6qp-sabresd.dtb by default. 

You can try pri fdtfile in uboot console to confirm it.

 

Regards

Harvey

0 Kudos
Reply

742 Views
gufengzi
Contributor III

how to use imx-image-full.env, rootfs.tar.zst, rootfs.wic.bmap, testdata.json, uboot-bootpart.wks?

0 Kudos
Reply