how to find iMX8QXP Silicon revision A0 / B0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to find iMX8QXP Silicon revision A0 / B0

跳至解决方案
1,527 次查看
Poons
Contributor II

Hi,

is there way to find iMX8QXP Silicon revision A0 / B0? please let us know.

Will boot loader start address (SD card Flashing address) depends on Silicon revision? please provide details on this.

Thanks in advance

Poons.

0 项奖励
回复
1 解答
1,513 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

You may identify the silicon revision by the marking if it ends in A correspond to rev A0, same goes for B and C revisions.

MiMX8QX6AVLFZAB indicates that it is an i.MX 8X B0 part

Regarding uboot offset you're correct, if the full SD/eMMC card image (.sdcard/.wic) is not used and copying the bootloader manually the offset for A0 revision is 33 while for B0 is 32

i.e. copying a i.MX 8X B0 part bootloader image

$ sudo dd if=<u-boot image> of=/dev/sdx bs=1k seek=32 conv=fsync

Best regards,
Aldo.

在原帖中查看解决方案

3 回复数
1,514 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

You may identify the silicon revision by the marking if it ends in A correspond to rev A0, same goes for B and C revisions.

MiMX8QX6AVLFZAB indicates that it is an i.MX 8X B0 part

Regarding uboot offset you're correct, if the full SD/eMMC card image (.sdcard/.wic) is not used and copying the bootloader manually the offset for A0 revision is 33 while for B0 is 32

i.e. copying a i.MX 8X B0 part bootloader image

$ sudo dd if=<u-boot image> of=/dev/sdx bs=1k seek=32 conv=fsync

Best regards,
Aldo.

864 次查看
mikeMJD
Contributor I

Sorry for reopening this, but Is there a way we can recover a board after flashing a bad image revision? We already attempted to use uuu and flash the correct one but it complains about [LIBUSB_ERROR_IO] SDPS: boot .bin-flash

0 项奖励
回复
853 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello @mikeMJD,

Please do help me by creating a new community thread so it may be easier to follow-up on your issue.

Anyway, taking a quick look I see that there is an space beetween boot and .bin if this is the case on the UUU command you have used, it may lead to issues when attempting to flash.

Regards,
Aldo.

0 项奖励
回复